This section is to set up the communication interface of the UPS. Please refer to the UPS manual to set the correct communication type. Any wrong settings will cause disconnection between the UPS and CS101.
Number of Batteries, Battery Full Charge Voltage (V), Battery Exhausted Charge Voltage (V)
Please refer to the UPS manual to set the value.
Date of last battery replacement (yyyy/mm/dd)
This section is to record the date when the UPS battery was last replaced.
Test UPS
Test UPS for every
This section is to schedule the UPS to test once a week or once every two weeks or not to test.
Test UPS on Weekday
This section is to set the UPS to test on a particular day of a week.
Start Time of UPS Testing (hh:mm)
This section is to set the UPS to test at a certain time on the test day.
UPS Test Type
This section is to select the type of self test to perform.
UPS Recorder
UPS Data Log
This section is to set how often the UPS data should be logged.
Warning Threshold Value
Time out of after lost of connection
This section is to set a period of time after which CS101 will send a disconnection warning message. This warning message will be sent after CS101 has lost contact with the UPS for the time specified.
Critical Load (%)
This section is to set the UPS critical loading. (shown as %) CS101 will send a warning message when the UPS is overloaded.
Critical Temperature (°C)
This section is to set the UPS critical internal temperature. CS101 will send warning messages when the UPS overheats.
Critical Capacity (%)
This section is to set the UPS critical battery capacity (shown as %) CS101 will send warning messages when UPS low battery occurs.
This page is to set the UPS configuration. Any wrong settings will cause incorrect display values or disconnection between the UPS and CS101.