| Miscellaneous |  |
|
Turn off UPS when AC power Fails |
It will turn off the UPS when the AC power fails. Is possible to reboot the UPS by selecting "Reboot UPS". |
Put UPS in Sleep mode for __ minutes |
When the UPS is put into Sleep mode, it will not provide power. The UPS will provide power again after Sleep mode time is complete. |
Wake Up UPS |
This function is to start up the UPS. |
Reboot UPS |
When execute such command, UPS load would start over. |
UPS Buzzer On/Off |
This is to turn on/ off the UPS buzzer. |
This page is to provide remote UPS test functions. Choose the test item, then click on 'Apply' to execute it. Please refer to the UPS manual for individual UPS Test functions. |