| Access Control |  |
|
Manager IP Address |
This section is to set the IP address that the administrator can manage CS101 from. It is valid for up to 8 IP addresses. To manage CS101 from any IP address, enter *.*.*.* into "Manager IP address". |
Version |
This section is to set SNMP versions. |
Community |
This section is to set a Community name for NMS. The community name has to be as the same as the setting in NMS. |
Permission |
This section is to set authorizations of administrators. Options are Read, Read/Write, and No Access. |
User Name |
This section is to set SNMP user's account (only if used SNMPv3). |
Password |
This section is to set SNMP user's password (only if used SNMPv3). |
Authentication |
This section is to select between MD5 or SHA (only if used SNMPv3). |
Privacy |
This section is to select between DES or AES (only if used SNMPv3). |
Description |
This section is for an administrator to make notes. |
 | Trap Notification |  |
|
Receiver IP Address |
This section is to set receivers IP address for receiving traps sent by CS101. It is valid for up to 8 IP addresses. |
Community |
This section is to set a Community name for NMS. The community name has to be as the same as the setting in NMS. |
Trap Type |
To select between PPC or RFC1628. |
Severity |
This section is to set Trap receiver levels. There are three levels of Trap receiver :
- Information: to receive all traps.
- Warning: to receive only "warning" and "severe" traps.
- Severe: to receive only "severe" traps.
Please refer to NMS manual for Trap levels.
|
Accept |
This section is to set to receive a Trap or not. |
Description |
This section is for an administrator to make notes. |
Event |
This section is to select events for CS101 to send traps. Clicking on Select will open a Select Events List. Event Traps may be selected from this list. |
This page is to set CS101 SNMP settings so it can be used by a NMS (Network Management System). |